Create or sign in to your account for the best pricing!

Your account pricing is now applied.

Toggle Nav
Search
My Cart

Electronic Overload Relays

We can't find products matching the selection.

Electronic Overload Relays for Motor Protection and Control

Electronic overload relays are used to protect electric motors from overload conditions, phase loss, phase imbalance, and other operating faults that can lead to overheating or equipment damage. Unlike traditional thermal overload devices, electronic overload relays use current sensing and electronic logic to provide more precise protection, faster response, and adjustable trip settings for motor control applications.

In industrial automation and control systems, electronic overload relays are commonly installed with motor starters, contactors, and control panels to monitor motor current and interrupt operation when unsafe conditions are detected. They are used in applications such as pumps, fans, conveyors, compressors, machine tools, and production equipment where reliable motor protection is essential. As part of a broader overload relay strategy, electronic models help improve system visibility, reduce nuisance tripping, and support more accurate protection across varying load conditions.

When selecting an electronic overload relay, key considerations include motor full-load current, trip class, phase configuration, reset method, communication capability, and compatibility with the contactor or starter being used. Additional features such as ground-fault detection, phase-loss protection, thermal memory, diagnostics, and remote reset may be important, depending on the application. Electronic overload relays are often integrated into broader automation and control systems that require equipment protection, monitoring, and coordinated shutdown.

Properly selected electronic overload relays help reduce downtime, extend motor service life, and improve the reliability of automated equipment. They provide a critical layer of protection for motor-driven systems while enabling safer, more efficient operation in industrial control environments.

Frequently Asked Questions

What is the difference between electronic and thermal overload relays?

Electronic overload relays use sensors and electronic logic to monitor current and provide adjustable protection. Thermal overload relays use heat-sensitive elements that respond to current-related temperature rise. Electronic models typically offer greater accuracy, wider adjustment ranges, diagnostics, and additional protection features.

How do I select the correct electronic overload relay?

Selection should be based on motor full-load current, supply voltage, phase configuration, trip class, contactor or starter compatibility, reset method, communication requirements, and any needed protection features such as ground fault or phase loss detection.

What is trip class on an electronic overload relay?

Trip class defines how quickly the overload relay trips under overload conditions. For example, a Class 10 relay trips faster than a Class 20 or Class 30 relay. The correct trip class depends on motor starting time and application requirements.