Conduit outlet bodies are used in electrical raceway systems to provide access points for pulling, splicing, changing direction, and terminating conduit runs. They help simplify installation and maintenance by creating a protected space where conductors can be accessed without disassembling larger sections of the conduit system. In industrial and commercial environments, conduit outlet bodies are commonly used where conduit changes direction or where access is needed for inspection and servicing.
Different types of conduit outlet bodies are designed for different routing and access needs. Some are used primarily to change conduit direction while maintaining pull access, while others are selected for service entrance applications or to protect conductor transitions. Related components such as covers and gaskets help maintain enclosure protection and keep the assembly properly sealed for the installation environment.
Galco offers conduit outlet body components for a range of industrial electrical applications. Choosing the correct option depends on conduit size, entry direction, available space, environmental exposure, and whether the application requires access for pulling conductors, changing direction, or making a service entrance connection. Proper selection helps support safer installation, easier maintenance, and more reliable conduit system performance.
Selection starts with the conduit layout and the purpose the outlet body needs to serve within the run. Conduit size and thread compatibility must match the rest of the system, but the body style is just as important because it determines how conductors enter, exit, and can be accessed later. Some applications need a body that primarily supports wire pulling around a change in direction, while others need a compact access point in a tight installation area or a configuration suited to service entrance use.
Installation environment also plays a role in choosing the right components. In locations exposed to dust, moisture, or weather, the correct combination of body, cover, and gasket helps maintain protection and enclosure integrity. Conduit outlet bodies are often used alongside other raceway hardware such as fittings and conduit mounts to support a complete conduit installation.
A conduit outlet body is used to provide access to conductors in a conduit run for pulling, inspection, maintenance, or directional changes. It helps create a protected access point without requiring larger sections of conduit to be removed or disassembled.
Start by matching the conduit size and thread type, then determine how the conduit run needs to enter and exit the body. It is also important to consider available installation space, whether future wire access is needed, and whether the application requires additional sealing components such as covers or gaskets.
Service entrance outlet bodies are typically used where conductors transition into a building or enclosure and added protection is needed at the entry point. The right style depends on conductor routing, environmental exposure, and the requirements of the overall conduit system.