Create or sign in to your account for the best pricing!

Your account pricing is now applied.

Toggle Nav
Search
My Cart

Phase Rotation Testers

We can't find products matching the selection.

A phase rotation tester is a test instrument that shows the direction a 3-phase motor will rotate when connected to its power source.

Phase rotation testers have three leads to connect to the input power supply. A small display identifies each lead - L1, L2, or L3 - and the direction the motor will rotate if it is connected the same way.

The tester helps ensure correct installation before a motor is installed, preventing damage in the event that the motor rotates in the wrong direction. If the tester reads the wrong motor direction, simply swap the two leads, test rotation, and connect the motor in that orientation.

Types of Phase Rotation Testers

Phase rotation testers help verify phase sequence in three-phase systems during installation and service. They are used when confirming correct phase rotation supports equipment setup and verification workflows.

  • Phase rotation testers designed for quick sequence checks during installation.
  • Portable testers intended for routine service and maintenance routes.
  • Models designed for clear results and repeatable verification steps.

For general three-phase electrical troubleshooting and numeric readings, compare multimeters. For quick verification checks without detailed values, compare electrical testers.

Key Selection Criteria for Phase Rotation Testers

  • Compatibility with the systems and connections you work with.
  • Clarity of results and ease of interpretation.
  • Usability in field environments, including portability and durability.
  • Handling and connection style that fits your workflow.
  • Any additional verification features needed for your service routines.

Selecting a tester matched to the application helps support efficient verification and consistent installation checks.

Frequently Asked Questions

Why is phase rotation verification important?

Verifying phase rotation helps confirm phase sequence in three-phase systems during installation and service workflows where correct setup is required. For complementary checks after installation, power monitoring can help validate behavior over time.

How do I choose a phase rotation tester for field work?

Compare compatibility and ease of connection first, then evaluate portability, durability, and clarity of results for the environments where you work. For broader electrical troubleshooting, compare multimeters.

What should I review before connecting a tester?

Confirm system compatibility and follow appropriate safety and connection procedures for your environment before performing verification checks. For quick verification tasks beyond phase sequence, compare electrical testers.