A resistance meter, or ohmmeter, is a testing instrument that measures electrical resistance. Most ohmmeters are digital devices, although analog variants are available for measuring rapidly fluctuating values.
Ohmmeters work by passing a constant current through the resistance, with a second circuit that measures voltage across that resistance. A microcontroller or microprocessor then uses Ohm's Law to divide the voltage by the current and display the resulting resistance value to the user.
Resistance meters are suitable for a huge variety of applications, from circuit testing on boards or small electronic devices, to insulation testing on motors, transformers, or other heavy machinery.
Resistance meters support troubleshooting and verification tasks where resistance readings are critical. They are used when resolution and repeatability are important for the measurement workflow.
For broader electrical measurements beyond resistance, compare multimeters. For quick verification checks without detailed measurements, compare electrical testers.
Selecting a resistance meter matched to the measurement need supports clearer troubleshooting and more consistent verification.
Use a resistance meter when resistance measurement is the primary requirement and when higher resolution or repeatability is important to the workflow. Use a multimeter for broader electrical measurements.
Focus on measurement range, resolution, accuracy, and repeatability. Then consider ease of connection and usability based on how the measurement is performed. For general electrical verification tools, compare test equipment.
Start with the expected resistance values in your application, then select a range that covers those values and a resolution that supports the level of detail you need. If you also document electrical behavior over time, compare power monitoring.